We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by SIEMENS
This SIMATIC Project SDC starter package offers an open, data centric and purely software-based automation runtime (SIMATIC Project SDC Instance) and key automation edge apps (SIMATIC Project SDC Control App ("SDC DCA") and SIMATIC Project SDC PROFINET App ("SDC PNA") as well as services for building industrial automation solutions with IT like methods and workflows.
SIMATIC Project SDC is available as an image for IPC, virtual machines, or cloud (each a "SDC Instance"). An SDC Instance can be deployed on either physical, virtualized hardware, or cloud and is managed as an Industrial Edge Device through Industrial Edge.*
Each SDC Instance can then be used to install either self-developed Industrial Edge Apps or to host SIEMENS Industrial Edge Apps.
To develop an automation solution using structured text according to IEC 61131-3, we recommend the SIMATIC Project SDC Control App.
Use the SIMATIC Project SDC OPC UA Server App ("SDC UAS") to make data available to a connected HMI.
*Onboarding and management of an Industrial Edge Device requires an Industrial Edge Device Management License.
This Offering entitles Customer to:
Siemens AG
Gleiwitzer Straße 555, 90475 Nürnberg