We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by axtesys GmbH
The axtesys MySQL Connector makes your Siemens Industrial Edge Device ready for transmitting and reading data from your MySQL Database anywhere in the world.
Reliability and System Stability
We ensure fail-safe transmission of your data via the data bus. A built-in buffer and the detection of a failure in the transmission ensure that none of your data is lost and that it is also correctly transmitted afterwards. The Siemens Industrial Edge Device continues to record the data from your machines, stores it temporarily and transfers it as soon as the connection is restored.
Simple Configuration
The simple configuration with the Siemens Common Configurator allows you to configure the application in the familiar interface you are already used to.
Multiple Data Base Connections
The MySQL Connector can simultaneously connect to various databases. Therefore, please choose the appropriate package to address all your databases through your Industrial Edge Devices.
Entitlement
The MySQL Connector can simultaneously connect to various databases. Therefore, please choose the appropriate package to address all your databases through your Industrial Edge devices. The number of connections refers to the potential amount of database connections per Industrial Edge Device.
Questions, suggestions or ideas?
Please don’t hesitate to contact us if you want to learn more about the axtesys MySQL Connector or if you have any suggestions or ideas to make the application even better!
Martin Leitgeb
Telephone: 0043 (0)660 655 9755
E-Mail: martin.leitgeb@axtesys.at