We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by SIEMENS
Insights Hub Edge Analytics is an edge application that collects and preprocesses high and low frequency data, corelates the data and performs out of the box analysis as well. Additionally, custom KPI calculations can be designed using a large library of analyzing functions.
Insights Hub Edge Analytics makes it possible to perform Condition Monitoring and as a result receive valuable information like the health status of machines or the performance of a production process. After preprocessing, the calculated data is then uploaded to Insights Hub.
Condition Monitoring is used for condition-based maintenance of machines, processes, and complete plants. The intention is to avoid unplanned downtimes to increase production line and plant availability. Therefore, a cyclic or permanent measurement and analysis of data is performed. Physical quantities could for example include temperature, speed, torque, vibration, pressure or current. Here the performance requirements regarding sensors and connectivity are usually very high. This applies especially to rotating equipment, where mechanical vibrations are used to determine the condition. The vibration signal provides information about the load of a machine and evolving faults. Streaming data from manufacturing machines, industrial equipment, and other connected devices creates a massive amount of data. Preprocessing and analysis at the edge provides cost benefits and reduces latency.
Edge Analytics provides:
Offering Overview
| Insights Hub Edge Analytics | Insights Hub Edge Analytics Data Points Upgrade |
|---|---|
| Access the Edge Analytics application in your Launchpad and configure and manage your edge devices for data collection and analysis at higher smapling rate, preprocessing high dynamic singals before sending output to Insights Hub | Configure 5 data points in your edge device for preprocessing |