We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by SIEMENS
The Connector for MTConnect is designed to seamlessly connect machine tools using the MTConnect protocol to Siemens Industrial Edge. This integration empowers manufacturers to harness the full potential of their machine data, enabling advanced analytics, real-time monitoring, and optimized operational processes.
Entitlement
A subscription for this Industrial Edge App entitles to:
| Minimum Quantity | Maximum Quantity | Discount per Quantity | Subscription Term |
|---|---|---|---|
| 0 | To 24 | Yearly | |
| 25 | To 49 | 5.00% | Yearly |
| 50 | To 99 | 10.00% | Yearly |
| 100 | To Max | 10.00% | Yearly |
Siemens AG
Frauenauracher Straße 80, 91056 Erlangen