We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Additional Requirements
Hardware requirements
Industrial Edge Device Management License
Industrial Edge Device via Industry Mall
Depending on the usecase further applications (free of charge) are required and recommended
IIH Registry Service (required for almost every usecase)
Common Configurator (required to configure connectors)
Common Import Converter (required for several tag import tasks)
IIH Essentials (required to store and structure data)
Provided by SIEMENS
Connectors are essential to collect data from various PLCs and devices and make it available on the Industrial Edge system.
With the Connector for LoRaWAN sensor data can be accessed via LoRaWAN Gateways.
This connector is developed as Connectivity Suite Connector and therefore supports standardized configuration as well as data transfer.
The Configuration of the Connector is done with the Common Configurator, which is available free of charge in the Industrial Edge marketplace.
Industrial Edge App developers and Industrial Edge App users can use the data in their own and existing applications and services. The Industrial Edge Connectors provide a unified data interface to reduce the development effort for Industrial Edge Apps and are the basis for innovative and modularized software solutions.
Entitlement
A subscription for this Industrial Edge App entitles to:
Volume Discounts: For bulk purchases and quantities over 100, you may please contact your Sales representative.
Minimum Quantity | Maximum Quantity | Discount per Quantity | Subscription Term |
---|---|---|---|
0 | To 24 | Yearly | |
25 | To 49 | 5.00% | Yearly |
50 | To 99 | 10.00% | Yearly |
100 | To Max | 10.00% | Yearly |
Siemens AG
Gleiwitzer Straße 555, 90475 Nürnberg
https://www.siemens.com/global/en/products/software/simatic-apps.html