We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by SIEMENS
A graphical design environment for creating harness and formboard drawings, Solid Edge Harness Design can be used for in-house production or build-to-print purposes. With an intuitive user interface that makes harness design authoring easy, the software automates many design tasks.�
For example, connector tables are automatically populated as wires are added, terminals selected, and wire tables generated. A powerful parts selector automatically configures and selects terminals, seals and wires for each connector, including allowances for add-ons and knock-offs. This speeds the harness design and eliminates the major source of problems found in the traditional design process.�
Once a harness is complete, powerful reporting capabilities can be used to generate the documentation required for manufacturing. The reports are generated directly from the design drawing, ensuring fast and accurate information. This can significantly reduce production lead times and prevent manufacturing errors.
Solid Edge Harness Design contains robust part and model repositories, which support the automated selection of parts, terminal plugs and seals for each connector. The parts library includes over 4,000 popular industrial parts.
The software supports the International Electrotechnical Commission (IEC) and American National Standards Institute (ANSI) symbol and parts libraries; ANSI ladder schematics adhere to ANSI drawing standards, which is especially useful when designing machinery.
Solid Edge Harness Design and Solid Edge Wiring Design, combined with the Solid Edge 3D Design environment, allow companies to bring products to market faster without sacrificing quality. When deployed together, Solid Edge Wiring Design reduces effort by automating the flow of wiring data into Solid Edge Harness Design. When used with Solid Edge Electrical Routing, this unique solution provides interactive, highlighted cross-probing and dynamic updating between the ECAD-MCAD domains, which helps minimize design errors and shortens development time. Solid Edge electrical design modules are available individually or as a bundled solution.
Teamcenter Share: Cloud-based collaboration
Your subscription also includes access to Teamcenter Share, a next-generation, cloud-based collaboration solution from Siemens. With capabilities including secure, central storage and e-mail address-based sharing, Teamcenter Share allows you to instantly, securely and easily collaborate with colleagues, partners and customers. An Enterprise Cloud Account (ECA) will be provided to you for administrators to gain access to Teamcenter Share and delegate additional privileges.
For Teamcenter Share cloud services, a limitation of 10 Authorized Users (including guest users) per collaboration project applies, unless Customer has purchased additional entitlements. Any volume of storage space noted above for Teamcenter Share is incremental to the floating storage of 500 GB available for use across all of Customer's current subscriptions which include Teamcenter Share cloud services and which are assigned to the same tenant. Numbers noted above for Authorized Users and storage for Teamcenter Share are not listed on a per quantity basis.
Except guest users, all Authorized Users of Teamcenter Share cloud services will receive access to "Getting Started with Siemens Xcelerator Academy" (LAAS49000) on-demand training on the Siemens Xcelerator Academy portal.