We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Provided by SIEMENS
Maximize shop floor efficiency with a single unified Computer-Aided Manufacturing (CAM) system. Avoid the need for and cost of multiple CAM systems in the machine shop with Solid Edge CAM Pro. The scalable solution offers a wide range of in-depth NC programming capabilities, providing flexibility and maximizing the value of your investment.
Solid Edge CAM Pro is easy to deploy, learn and use. The Solid Edge CAM Pro 3-Axis Bundle stands out for its amazing range of features and capabilities � providing everything you need in a CAM solution. This 3-Axis bundle includes CAD and CAM for one low price.
Adaptive Roughing
Adaptive roughing allows your CNC to make parts faster, optimizes your machine operation, and extends the life of your cutting tools. This functionality is included in our 3-Axis bundle at no extra charge and can safely handle pillar removal and bottom-up cutting.
Model Associativity
Data sent to Solid Edge CAM Pro from your Computer-Aided Design (CAD) system retains associativity so that late-stage design changes can be easily incorporated into the manufacturing plan. Solid Edge CAM Pro includes industry translators that can read data in the native format of practically any CAD system, maintaining a high level of associativity regardless of the geometry source.
Intelligent Tool Paths
Solid Edge CAM Pro includes built-in tool path visualization and material removal verification tools. Integrated collision checking identifies any possible problems. You can also make fast changes to tool path results with graphical editing tools and protect your edits by locking tool paths from future re-calculations. No need for third-party visualization or machining simulation software.
In-Process Workpiece (IPW)
The In-Process Workpiece (IPW) feature shows the state of the machined model during the machining process. Solid Edge CAM Pro can automatically save the IPW at any point in the process. The IPW feature in Solid Edge CAM Pro follows the model as it gets machined, which saves time as the software knows what has been cut already. No time is wasted on �air-cutting�.
Post Hub Library
Included with Solid Edge CAM Pro, the Post Hub library enables a streamlined process to generate production-ready CNC programs for your applications. Post Hub lets you access more than 1,300 postprocessors directly from CAM Pro, search by key machine characteristics and download directly to your workstation.
Your Solid Edge CAM Pro 3-Axis Bundle subscription includes: