We realized that your billing location is USA.
Please note that your billing address should be in the same country as your buying location. Please select one of the options:
The Subscription Term will automatically renew for successive Subscription Terms unless either party notifies the other at least 60 days prior to the end of the then-current Subscription Term that it has elected not to renew. Any renewed Subscription Term will be the same length as the preceding term or 12 months, whichever is greater. The fees for any renewed Subscription Term will be the same as those in effect at the end of the preceding Subscription Term, unless Siemens notifies Customer about different future fees at least 90 days prior to the end of the then-current Subscription Term.
The UCA (or any successor terms) available at Universal Customer Agreement (UCA) in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term. However, if your subscription is governed by a master agreement that you have executed with Siemens, then that master agreement will continue to apply for any following Subscription Term, and auto-renewal terms for the subscription specified in that master agreement will prevail.
In all cases, instead of any previous versions of Supplemental Terms, the applicable Supplemental Terms available at Supplemental Terms in the version that is current 60 days prior to the end of the then-current Subscription Term will apply for the following Subscription Term.
Additional terms and conditions agreed upon in the initial order form (including product-specific terms), as well as agreed payment terms, will remain in effect for any following Subscription Term.
Prerequisites
Industrial Edge Hub Access
Additional Requirements
Hardware Demands
Siemens Industrial Edge Device Management License
Siemens Industrial Edge Device via Industry Mall
Provided by SIEMENS
Do you see AI as a potential solution for your current challenges?
But are you concerned about the high costs and effort to bring AI to the shop floor and maintain it?
Are you interested in standardizing the execution of AI Models on the shop floor and integrate it with monitoring, debugging, and remote deployment capabilities?
AI Inference Server is the edge application to standardize AI model execution on Siemens Industrial Edge. The application eases data ingestion, orchestrates data traffic, and is compatible all powerful AI frameworks thanks to the embedded Python interpreter. It enables the AI model deployment as content to a standard edge app instead of custom container deployment for single models. AI finally meets Siemens Industrial Edge and AI Inference Server leverages the benefits of both.
Entitlement
You can choose from several AI Inference Server variants which have different hardware requirements*
AI Inference Server - 1 pipeline
Allows single execution of one pipeline.
AI Inference Server - 3 pipelines
Allows the execution up to three pipelines at the same time.
AI Inference Server GPU accelerated
AI Inference Server GPU accelerated application is taking advantage of the high-performance GPU computation. It allows single execution of 1 pipeline on a GPU accelerated hardware device.
* please find the hardware requirements on the left side.
Only one AI Inference Server application instance (from the above list) can be installed on an edge device.
It means you can install AI Inference Server or AI Inference Server - 3 pipelines or AI Inference Server GPU accelerated on a single edge device.
You cannot install e.g. AI Inference Server and AI Inference Server GPU accelerated applications on a single device.
Siemens AG
DI FA CTR SVC&AI IAI
Siemenspromenade 1
91058 Erlangen, Germany
Copyright © Siemens AG, [2023], and licensors. All rights reserved.